U bent hier  :  home  ››  nieuws  ››  productnieuws  ››  LAMBDA SHOWS INNOVATIONS IN PO...

U kunt ook op de volgende manier contact met ons opnemen:

LAMBDA SHOWS INNOVATIONS IN POWER AT SOUTHERN ELECTRONICS

Geplaatst : 03 Jan 2007

Lambda UK
Stand D25
Southern Electronics 2007
Thorpe Park, Surrey
7th – 8th February 2007


At Southern Electronics 2007, Lambda is showcasing an extensive family of new products, ranging from tiny board-mounting DC/DC converters to multi-kilowatt power supplies. Following Lambda’s acquisition by TDK Corporation of Japan, a range of new products designed and manufactured under the collaborative TDK-Lambda brand will be featured.

Martin Southam, Director of Marketing for Lambda Europe said of the event, “Southern Electronics is our first opportunity to show our expanded range of new products, available since becoming part of TDK in the UK. Lambda is now exclusively marketing TDK power supplies to Industrial, Medical and Instrumentation customers in the UK.”

“The new organisation combines leading-edge power supply design expertise with TDK’s recognised advanced component technology,” he continued, “This combination means that we are now in a strong position to provide our customers with the very best in power solutions, as a visit to our stand will quickly confirm.”

Highlights on the Lambda stand include NV300 watt and 700 watt 1U configurable power supplies which offer high power density to save space, and high efficiency which not only minimises the generation of unwanted heat but also reduces wasted power.
Plus, the new PFE 500 and 700 watt front end models aimed at distributed power applications and rapid custom applications when combined with Lambda’s extensive range of DC bricks and POL converters.

Also on show are the new ultra-thin convection cooled RTW single-output supplies that are 50% smaller than typical products of a similar rating; CC-E series 1.5W to 25W DC/DC converters which combine a small footprint, low height, high efficiency and through hole or SMD mounting. The leading edge TDK Innoveta range of DC/DC bricks and POL converters will also be exhibited by Lambda for the first time.

Throughout the exhibition, experts from Lambda are on stand to demonstrate the new products and to give advice on the significant benefits, including cost of ownership savings, that ground-breaking power supply technology from Lambda and TDK can provide in the visitors’ own applications.

PAGE TOP

PAGE TOP