Sie sind hier  :  home  ››  presse  ››  produkt-news

Gerne können Sie uns auch telefonisch oder per E-Mail erreichen!

TDK-Lambda News

Produkt-News

Filter:8

Welcome to the TDK-Lambda news room. Here you'll find all of our product news and corporate announcements. You can also visit our news website for additional TDK-Lambda news.

Lambda's new SWS series makes high reliability and high performance more affordable

veröffentlicht : 01 May 2003

World-leading power supply manufacturer Lambda is introducing a new series of AC-DC power supplies that is ideal for cost-sensitive applications that require both high reliability and high performance.

mehr dazu

Lambda boosts the power of its half-brick DC-DC converter to 300w

veröffentlicht : 01 May 2003

Lambda continues to drive up the power density of its PAH family of ‘half-brick’ DC-DC power modules with the introduction of the new PAH300S48 with output voltages of 28 or 12V DC and 300W of power from a single output.

mehr dazu

Lambda Quarter-Brick PAQ a bigger punch

veröffentlicht : 01 Mar 2003

Technological advancement in DC-DC converters is continuing apace at Lambda as shown by the new PAQ100H range, the company’s most efficient, highest power quarter-brick DC-DC to-date.

mehr dazu

New Tarka range of non-isolated DC-DC Converters is first choice for point-of-load power needs

veröffentlicht : 01 Mar 2003

The Tarka range is a new generation of non-isolated DC-DC converters from leading global power solutions provider Lambda. The first model to be unveiled is the PL10, a 5V input, 10A output single-in-line packaged unit.

mehr dazu

New Lambda 20W unpotted DC-DC Converter provides cost-effective solution for low power intermediate

veröffentlicht : 01 Feb 2003

Lambda has unveiled an unpotted version of its X Series of industry standard 2 x 1 sized DC-DC converters. The new 20W UX20 allows designers to take full advantage of forced-air cooling to achieve higher output powers over a wider temperature range.

mehr dazu

PAGE TOP

PAGE TOP