Filters:3

Welcome to the TDK-Lambda news room. Here you'll find all of our product news and corporate announcements. You can also visit our news website for additional TDK-Lambda news.

NVM175 medical power supplies from TDK-Lambda

תאריך פרסום : 30 Mar 2010

TDK-Lambda introduces the NVM175 range of medically-approved AC-DC power supplies.

עוד

LEDסדרה חדשה של ספקי כוח לאפליקציות ה

תאריך פרסום : 08 Feb 2010

Dסדרה חדשה של ספקי כוח לאפליקציות LED

עוד

קטלוג ספקי כוח מותאם לדרישת לקוח

תאריך פרסום : 01 Feb 2010

קטלוג חדש- ספקי כוח המותאמים לדרישות לקוח

עוד

Ultra-compact 15W & 30W DC-DC ממירי מתח - TDK-Lambda

תאריך פרסום : 20 Jan 2010

Single output units boast efficiency up to 92.5% TDK-Lambda has extended its CC-E range of high efficiency, high reliability DC-DC converters with the introduction of new 15W and 30W versions

עוד

30-100W DC-DC converters from TDK-Lambda address railway applications

תאריך פרסום : 14 Dec 2009

Global power supply manufacturer TDK-Lambda has expanded its DC-DC converter line-up with the introduction of the new CN-A Series that have a wide range 60 -160VDC input, which is widely used in railway applications

עוד

Low power DIN-rail DC-DC converters from TDK-Lambda

תאריך פרסום : 08 Dec 2009

To satisfy customer demand for low power DC-DC converters that can be rapidly mounted onto DIN rails, TDK-Lambda has introduced the DPX Series

עוד

12W IP66-rated LED power supplies from TDK-Lambda

תאריך פרסום : 06 Oct 2009

TDK-Lambda has developed a new range of power supplies specifically targeted towards LED applications requiring high reliability. 

עוד

ספקי כוח לתאורת לד

תאריך פרסום : 06 Oct 2009

סדרת ספקי כוח חדשה המיועדת לתאורת הלד

עוד

TDK-Lambda introduces 1kW single-output power supplies in 1U format

תאריך פרסום : 30 Sep 2009

TDK-Lambda introduces 1kW single-output power supplies in 1U format

עוד

TDK-Lambda extends NV-Power’s reach

תאריך פרסום : 08 Sep 2009

TDK-Lambda has expanded its innovative NV-Power family of configurable AC-DC power supplies with the addition of four new output modules

עוד

TDK-Lambda augments EFE medical range with 28V, 40V and 48V models

תאריך פרסום : 01 Sep 2009

TDK-Lambda augments EFE medical range with 28V, 40V and 48V models

עוד

TDK-LAMBDA PUTS THREE-PHASE POWER ON THE RAIL

תאריך פרסום : 30 Jun 2009

To complement its already highly successful DPP range of DIN-Rail power supplies, TDK-Lambda has introduced three-phase input models.

עוד

TDK-LAMBDA QUARTER BRICKS MEET POWER-HUNGRY, ATCA REQUIREMENTS

תאריך פרסום : 28 Apr 2009

TDK-Lambda has expanded its DC-DC converter line-up with the introduction of the new iQG Series, providing exceptionally high true useable power in an industry standard quarter-brick footprint.

עוד

DESIGN WITH THE LATEST POWER INNOVATIONS USING

תאריך פרסום : 30 Mar 2009

TDK-Lambda, the innovator in power supply development, has launched its new power products catalogue for 2009

עוד

TDK-LAMBDA EXPANDS iHG FAMILY OF DOSA HALF BRICKS

תאריך פרסום : 23 Mar 2009

Following on from the successful launch of the iHG Series of half brick DC-DC converters, TDK-Lambda has added new devices offering a wide input range (36-75V) with nominal outputs from 2.5V/80A (200W), 3.3V/30A (99W), 3.3V/70A (231W), 5V/10A (50W) and 5V/60A (300W).

עוד

Latest 25W and 35W single output supplies from TDK-Lambda

תאריך פרסום : 09 Feb 2009

Following on from the successful launch of the LS Series of convection cooled, single output power supplies, TDK-Lambda has added the 25W and 35W models

עוד

CHALLENGES OF SPACE-SAVING POWER SUPPLIES FOR HARSH ENVIRONMENTS

תאריך פרסום : 19 Jan 2009

Operating reliably in extreme ambient temperatures is no small task for AC to DC power supplies with PFC, says David Buck of TDK-Lambda Europe, especially when they are employed in indoor and outdoor-mounted electronic equipment where compact size is mandatory

עוד

ADVANCES IN POWER SUPPLIES FOR AUTOMATED ELECTROCHEMICAL MINI-PLANTS

תאריך פרסום : 19 Jan 2009

On-site and on-demand production of disinfectants, biocides and water purification chemicals including sodium hypochlorite, chlorine dioxide has been substantially improved via the use of advanced switchmode power supplies that provide the power for automated electrochemical generators

עוד

TDK-LAMBDA’S AC INPUT FULL-BRICKS TAKE EFFICIENCY TO THE NEXT LEVEL

תאריך פרסום : 12 Jan 2009

Following the success of the PFE range of AC-DC full-brick power supplies, TDK-Lambda has introduced the PFE-S series with enhanced circuitry to improve lightning surge capability (up to 6kV) and line interrupt hold-up time

עוד

1 X 1 INCH DC-DC CONVERTERS POWER UP TO 15W

תאריך פרסום : 05 Dec 2008

TDK-Lambda has added two new models to its already succesful PX family of single- and dual-output 15W DC-DC converters

עוד

PAGE TOP

PAGE TOP