אתה נמצא כאן  :  בית  ››  חדשות  ››  חדשות המוצר  ››  Genesys™ family of programmabl...

פניה ישירה למענה מהיר


אני:

לחלופין, צור אתנו קשר בערוצים הבאים:

אם אינך בטוח איזה מוצר אתה זקוק, נסה את שלנו חיפוש מוצרים

Genesys™ family of programmable DC power supplies pack 5kW in 2U

תאריך פרסום : 10 Oct 2007

The Genesys™ family of programmable power supplies from Lambda sets a new standard for flexible, reliable, AC-DC power systems in OEM, industrial and laboratory applications. Lambda’s new 5kW module offers one of the highest power densities available in a compact 2U unit, and complements the already highly successful 1U 750W half-rack, 1U 750W/1.5kW, 2U 3.3kW and 3U 10kW/15kW full-rack models.

The new GEN 5kW power supply is offered as a full line up with 12 versions, The first group of 5kW models released including output voltage ranges of 0-8, 0-60, 0-150 and 0-600V. Maximum output current for the lowest voltage range is 600A. A wide choice of three phase AC inputs (either 208V or 400V) is available and all units have active power factor correction.Further models will be released during the first half of 2008.

A long list of standard features are common to the whole Genesys™ family including the built-in RS232/RS485 interface, along with comprehensive remote programming functions such as global commands for multiple power supply systems. External analogue programming and monitoring is user selectable from 0-5V and 0-10V. System designers will also benefit from the new high-speed status monitoring feature for the RS485 bus.

Test system customers using the IEEE-488.2 bus may achieve significant cost savings by incorporating the optional IEEE multi-drop interface card for a master unit, which can relay commands to up to 30 “slaves” via the standard RS485 links. Isolated analogue interface and LXI compliant LAN option cards are also available.

Higher power systems can be configured with up to four 5kW modules. Paralleling units for higher power is simplified with the master unit able to report total system output current, and rack space is minimised because all Genesys™ units are true “zero stack” with no space required between units.

CE marked in accordance with the Low Voltage Directive, Genesys™ conducted and radiated EMI conforms to EN55022-A, FCC-A. Safety approvals include UL60950 and EN60950. All models carry a five-year warranty.

PAGE TOP

PAGE TOP