Gerne können Sie uns auch telefonisch oder per E-Mail erreichen!
Welcome to the TDK-Lambda news room. Here you'll find all of our product news and corporate announcements. You can also visit our news website for additional TDK-Lambda news.
veröffentlicht : 18 Dec 2006
Lambda has expanded its highly successful NV–Power configurable power supplies line up with the addition of two new model ranges.
mehr dazuveröffentlicht : 27 Nov 2006
Ultra-thin convection cooled single-output power supplies in the new RTW range from the new collaborative TDK
mehr dazuveröffentlicht : 27 Nov 2006
Just 4.5mm high, the latest CE-10xx range of low-profile surface mount, non-isolated point of load DC/DC converters designed and manufactured by TDK are now available from power supply specialists, Lambda under the new collaborative TDK - Lambda product brand.
mehr dazuveröffentlicht : 27 Nov 2006
The MTW series of multi-output power supplies designed and manufactured by TDK are available from power supply specialists Lambda, under the new collaborative TDK - Lambda product brand.
mehr dazuveröffentlicht : 27 Nov 2006
Offering space savings of up to 50% compared with previous solutions, Lambda’s innovative new PFE-series AC-input ‘full brick style’ power supply modules.
mehr dazuveröffentlicht : 09 Oct 2006
Extending its DPP range of DIN-Rail power supplies to include new high power models is Lambda.
mehr dazuveröffentlicht : 04 Oct 2006
Power Supply expert Lambda now provides a truly comprehensive range of products with the addition of the TDK Innoveta family of DC-DC converters following Lambda's acquisition by TDK last year.
mehr dazuveröffentlicht : 02 Oct 2006
Just 56mm deep, the new low-profile DSP DIN-rail mounting power supplies from Lambda are specifically designed for easy installation in the shallow cabinets commonly used in building automation and security applications.
mehr dazuveröffentlicht : 11 Sep 2006
Lambda, the specialist power supply manufacturer, has launched its new power products catalogue for 2006/2007.
mehr dazuveröffentlicht : 04 Sep 2006
The latest CC-E compact DC/DC converters designed and manufactured by TDK are now available from power supply specialists, Lambda under the new collaborative TDK - Lambda product brand.
mehr dazuveröffentlicht : 18 Jul 2006
Lambda, the specialist power supply manufacturer, has now extended it’s industry leading HWS family of compact single-output power supplies to include models that are approved for use in medical equipment.
mehr dazuveröffentlicht : 11 Jul 2006
Two new families of very competitively priced filters from Lambda UK make it easy and inexpensive for engineers to enhance the EMC performance of almost any type of electronic equipment.
mehr dazuveröffentlicht : 07 Jul 2006
Designed to deliver high reliability even in harsh operating conditions, single-output industrial power supplies in the new LZSa series from Lambda combine rugged mechanical construction with an enhanced thermal design that allows them to operate over the exceptionally wide temperature range of -40ºC to +71ºC.
mehr dazuveröffentlicht : 25 Apr 2006
The specification of power supplies for medical applications is a task which needs to be approached with care. In particular, as Andy Skinner of Lambda UK explains, it is never safe to make assumptions about the suitability of power supplies which were primarily designed for industrial use.
mehr dazuveröffentlicht : 11 Apr 2006
Lambda, the leading global power supply manufacturer, has announced that, after extensive testing, its compact NV-175 and NV-350 multi-output power supplies have been granted approval in line with the stringent demands of US military standard, Mil-Std-801E.
mehr dazuveröffentlicht : 27 Mar 2006
Start collaboration with co - marketing activities to enhance power-supply business.
mehr dazuveröffentlicht : 20 Mar 2006
The new integral-fan version of Lambda UK’s ( www.lambda-europe.com) popular NV-175 compact multi-output power supply can deliver its full rated output power continuously, at ambient temperatures as high as 50ºC, even when there is no external source of cooling air flow.
mehr dazuveröffentlicht : 28 Feb 2006
Lambda UK has launched a new version of its FPS1000 front end power supply with a nominal output voltage of 32V adjustable from 28.8 to 38.4.
mehr dazuveröffentlicht : 20 Feb 2006
This must be a question most component engineers and purchasers are asking themselves as the RoHS directive implementation date of July 2006 approaches.
mehr dazuveröffentlicht : 24 Jan 2006
Lambda has added a new 3.3kW version of its successful Genesys™ range of rack-mountable, programmable power supplies.
mehr dazu