Sie sind hier  :  home  ››  presse  ››  produkt-news

Gerne können Sie uns auch telefonisch oder per E-Mail erreichen!

TDK-Lambda News

Produkt-News

Filter:4

Welcome to the TDK-Lambda news room. Here you'll find all of our product news and corporate announcements. You can also visit our news website for additional TDK-Lambda news.

NEW SURFACE MOUNT POL CONVERTERS HAVE WIDE-RANGE INPUTS

veröffentlicht : 03 Apr 2007

Ideal for point-of-load use, surface-mount DC/DC converters, the new CE-1050 range from Lambda.

mehr dazu

LAMBDA PACKS 450 WATTS INTO HALF A BRICK!

veröffentlicht : 01 Apr 2007

In response to customer demand for smaller and more cost-effective power sources, Lambda has introduced its innovative new range of PAH450 DC/DC converters.

mehr dazu

EFFICIENCY VERSUS EMC – A TRADE-OFF ELIMINATED

veröffentlicht : 14 Mar 2007

Whatever the application, power supply users want products that are small and efficient, yet have excellent EMC performance.

mehr dazu

LAMBDA SHOWS INNOVATIONS IN POWER AT SOUTHERN ELECTRONICS

veröffentlicht : 03 Jan 2007

At Southern Electronics 2007, Lambda is showcasing an extensive family of new products, ranging from tiny board-mounting DC/DC converters to multi-kilowatt power supplies.

mehr dazu

POWER SUPPLIES FOR INDUSTRY

veröffentlicht : 20 Dec 2006

With most industrial automation systems now based on equipment that operates at low voltages – typically 24V DC – there’s a big demand for power supplies for use in tough industrial applications.

mehr dazu

ELECTRONICA SEES LAMBDA EXPAND ITS NV-POWER PRODUCT RANGE

veröffentlicht : 18 Dec 2006

Lambda has expanded its highly successful NV–Power configurable power supplies line up with the addition of two new model ranges.

mehr dazu

THIN SUPPLY DELIVERS POWER IN HALF THE SPACE

veröffentlicht : 27 Nov 2006

Ultra-thin convection cooled single-output power supplies in the new RTW range from the new collaborative TDK

mehr dazu

LOW PROFILE SMD POINT OF LOAD CONVERTERS FEATURE ADJUSTABLE OUTPUTS

veröffentlicht : 27 Nov 2006

Just 4.5mm high, the latest CE-10xx range of low-profile surface mount, non-isolated point of load DC/DC converters designed and manufactured by TDK are now available from power supply specialists, Lambda under the new collaborative TDK - Lambda product brand.

mehr dazu

NEW TRIPLE OUTPUT LAMBDA POWER SUPPLIES ARE 26MM HIGH

veröffentlicht : 27 Nov 2006

The MTW series of multi-output power supplies designed and manufactured by TDK are available from power supply specialists Lambda, under the new collaborative TDK - Lambda product brand.

mehr dazu

LAMBDA’S SPACE-SAVING AC INPUT POWER MODULES HAVE HIGH TEMPERATURE CAPABILITY

veröffentlicht : 27 Nov 2006

Offering space savings of up to 50% compared with previous solutions, Lambda’s innovative new PFE-series AC-input ‘full brick style’ power supply modules.

mehr dazu

LAMBDA PUTS MORE POWER ON THE RAIL

veröffentlicht : 09 Oct 2006

Extending its DPP range of DIN-Rail power supplies to include new high power models is Lambda.

mehr dazu

NOW LAMBDA HAS ALL THE CONVERTERS YOU’LL EVER NEED!

veröffentlicht : 04 Oct 2006

Power Supply expert Lambda now provides a truly comprehensive range of products with the addition of the TDK Innoveta family of DC-DC converters following Lambda's acquisition by TDK last year.

mehr dazu

LAMBDA’S NEW LOW PROFILE DIN RAIL POWER SUPPLIES FIT THE BOX FOR BUILDING AUTOMATION

veröffentlicht : 02 Oct 2006

Just 56mm deep, the new low-profile DSP DIN-rail mounting power supplies from Lambda are specifically designed for easy installation in the shallow cabinets commonly used in building automation and security applications.

mehr dazu

LAMBDA LAUNCHES NEW PRODUCT CATALOGUE

veröffentlicht : 11 Sep 2006

Lambda, the specialist power supply manufacturer, has launched its new power products catalogue for 2006/2007.

mehr dazu

LAMBDA NOW OFFERS TDK DC/DC CONVERTERS

veröffentlicht : 04 Sep 2006

The latest CC-E compact DC/DC converters designed and manufactured by TDK are now available from power supply specialists, Lambda under the new collaborative TDK - Lambda product brand.

mehr dazu

LAMBDA ADDS MEDICAL AND HEAVY DUTY VERSIONS TO HWS POWER SUPPLY RANGE

veröffentlicht : 18 Jul 2006

Lambda, the specialist power supply manufacturer, has now extended it’s industry leading HWS family of compact single-output power supplies to include models that are approved for use in medical equipment.

mehr dazu

LAMBDA BOOSTS EMC PERFORMANCE FOR LESS

veröffentlicht : 11 Jul 2006

Two new families of very competitively priced filters from Lambda UK make it easy and inexpensive for engineers to enhance the EMC performance of almost any type of electronic equipment.

mehr dazu

LAMBDA HAS TOUGH SUPPLIES FOR INDUSTRY

veröffentlicht : 07 Jul 2006

Designed to deliver high reliability even in harsh operating conditions, single-output industrial power supplies in the new LZSa series from Lambda combine rugged mechanical construction with an enhanced thermal design that allows them to operate over the exceptionally wide temperature range of -40ºC to +71ºC.

mehr dazu

SUPPLYING THE POWER FOR MEDICINE

veröffentlicht : 25 Apr 2006

The specification of power supplies for medical applications is a task which needs to be approached with care. In particular, as Andy Skinner of Lambda UK explains, it is never safe to make assumptions about the suitability of power supplies which were primarily designed for industrial use.

mehr dazu

COMPACT SUPPLIES FROM LAMBDA MEET MILITARY SPECS!

veröffentlicht : 11 Apr 2006

Lambda, the leading global power supply manufacturer, has announced that, after extensive testing, its compact NV-175 and NV-350 multi-output power supplies have been granted approval in line with the stringent demands of US military standard, Mil-Std-801E.

mehr dazu

PAGE TOP

PAGE TOP