Gerne können Sie uns auch telefonisch oder per E-Mail erreichen!
Some low power supplies have what is termed a hiccup current-limit feature. As the name implies, if a current limit is sensed, the supply will reduce its output voltage to zero and then, after a short time, it will attempt to provide its normal voltage. These On-Off attempts at operation are referred to as a hiccup-mode. Should the overload condition be removed, the supply will again operate normally.