U bent hier  :  home  ››  nieuws  ››  productnieuws

U kunt ook op de volgende manier contact met ons opnemen:

TDK-Lambda Nieuws

Productnieuws

Filters:3

Welcome to the TDK-Lambda news room. Here you'll find all of our product news and corporate announcements. You can also visit our news website for additional TDK-Lambda news.

TDK-LAMBDA PUTS THREE-PHASE POWER ON THE RAIL

Geplaatst : 30 Jun 2009

To complement its already highly successful DPP range of DIN-Rail power supplies, TDK-Lambda has introduced three-phase input models.

Lees verder

TDK-LAMBDA SHOWCASES POWER INNOVATIONS AT NEW

Geplaatst : 12 May 2009

TDK-Lambda UK, one of the world’s leading power supply manufacturers, is showcasing an extensive array of new and innovative products, ranging from tiny board-mounting DC-DC converters to multi-kilowatt power supplies, at this year’s National Electronics Week.

Lees verder

TDK-LAMBDA QUARTER BRICKS MEET POWER-HUNGRY, ATCA REQUIREMENTS

Geplaatst : 28 Apr 2009

TDK-Lambda has expanded its DC-DC converter line-up with the introduction of the new iQG Series, providing exceptionally high true useable power in an industry standard quarter-brick footprint.

Lees verder

DESIGN WITH THE LATEST POWER INNOVATIONS USING

Geplaatst : 30 Mar 2009

TDK-Lambda, the innovator in power supply development, has launched its new power products catalogue for 2009

Lees verder

TDK-LAMBDA EXPANDS iHG FAMILY OF DOSA HALF BRICKS

Geplaatst : 23 Mar 2009

Following on from the successful launch of the iHG Series of half brick DC-DC converters, TDK-Lambda has added new devices offering a wide input range (36-75V) with nominal outputs from 2.5V/80A (200W), 3.3V/30A (99W), 3.3V/70A (231W), 5V/10A (50W) and 5V/60A (300W).

Lees verder

Latest 25W and 35W single output supplies from TDK-Lambda

Geplaatst : 09 Feb 2009

Following on from the successful launch of the LS Series of convection cooled, single output power supplies, TDK-Lambda has added the 25W and 35W models

Lees verder

CHALLENGES OF SPACE-SAVING POWER SUPPLIES FOR HARSH ENVIRONMENTS

Geplaatst : 19 Jan 2009

Operating reliably in extreme ambient temperatures is no small task for AC to DC power supplies with PFC, says David Buck of TDK-Lambda Europe, especially when they are employed in indoor and outdoor-mounted electronic equipment where compact size is mandatory

Lees verder

ADVANCES IN POWER SUPPLIES FOR AUTOMATED ELECTROCHEMICAL MINI-PLANTS

Geplaatst : 19 Jan 2009

On-site and on-demand production of disinfectants, biocides and water purification chemicals including sodium hypochlorite, chlorine dioxide has been substantially improved via the use of advanced switchmode power supplies that provide the power for automated electrochemical generators

Lees verder

TDK-LAMBDA POWERS UP FOR 2009 AT SOUTHERN MANUFACTURING & ELECTRONICS

Geplaatst : 13 Jan 2009

At this year’s Southern Manufacturing & Electronics show, visitors to the TDK-Lambda stand (C37) will discover all the latest advances and innovations in power technology

Lees verder

TDK-LAMBDA’S AC INPUT FULL-BRICKS TAKE EFFICIENCY TO THE NEXT LEVEL

Geplaatst : 12 Jan 2009

Following the success of the PFE range of AC-DC full-brick power supplies, TDK-Lambda has introduced the PFE-S series with enhanced circuitry to improve lightning surge capability (up to 6kV) and line interrupt hold-up time

Lees verder

1 X 1 INCH DC-DC CONVERTERS POWER UP TO 15W

Geplaatst : 05 Dec 2008

TDK-Lambda has added two new models to its already succesful PX family of single- and dual-output 15W DC-DC converters

Lees verder

TDK-LAMBDA LAUNCHES FIRST 1000W AC-DC POWER BRICKS

Geplaatst : 28 Nov 2008

TDK-Lambda adds more functionality to its PFE range of AC-DC MEGA-brick power supplies with the introduction of the 1000W PFE-F Series

Lees verder

TDK-LAMBDA EXTENDS QUARTER BRICK LINE

Geplaatst : 06 Nov 2008

TDK-Lambda has further extended its impressive line up of high power quarter brick modules with the introduction of the iQL Series

Lees verder

DIGITAL CONTROL POWER SUPPLIES FROM TDK-LAMBDA

Geplaatst : 27 Oct 2008

TDK-Lambda has extended its revolutionary digital power supply technology to include a new range of models designed specifically with medical applications in mind

Lees verder

TDK-LAMBDA TAKES DIGITAL CONTROL TO THE NEXT LEVEL

Geplaatst : 09 Oct 2008

Taking digital control to the next level, TDK-Lambda’s revolutionary EFE Series of embedded frontend power supplies delivers industry leading power density, high efficiency and enhanced reliability

Lees verder

LAMBDA PACKS 2.4kW INTO A 1U RACK

Geplaatst : 29 Jul 2008

Lambda has added a new 1U 2.4kW version to its successful Genesys™ range of rack-mountable, programmable power supplies that cover 1U, 2U and 3U formats

Lees verder

LAMBDA SHOWS ITS FULL POWER AT SOUTHERN ELECTRONICS

Geplaatst : 17 Jul 2008

Lambda UK is showcasing an extensive display of new products, ranging from tiny board-mounting DC-DC converters to multi-kilowatt power supplies, at Southern Electronics 2008.

Lees verder

LAMBDA'S PFE500F BRINGS MORE FUNCTIONALITY TO THE PFE SERIES

Geplaatst : 17 Jul 2008

Lambda has extended its PFE series of AC-DC full-brick power modules with the introduction of the PFE500F with additional features including active current sharing and remote on/off. Like the existing PFE300, PFE500 and PFE700 models, the new PFE500F versions provide a convenient ac-dc board mounted solution for applications – such as industrial, datacom and telecom – but bring further functionality.

Lees verder

POWER SUPPLIES AND CONDUCTED EMISSIONS – 10 QUESTIONS ANSWERED

Geplaatst : 17 Jul 2008

What EMC considerations should an engineer take into account when designing in a power supply? Stuart Nottage and Rob Hutton of Lambda UK give their advice.

Lees verder

LAMBDA EXHIBITS AT NATIONAL ELECTRONICS WEEK

Geplaatst : 17 Jul 2008

Lambda UK Stand E60 National Electronics Week Earls Court, London 17th – 19th June, 2008

Lees verder

PAGE TOP

PAGE TOP