Siete qui  :  home  ››  notizie  ››  news di prodotto

In alternativa, puoi contattarci così:

TDK-Lambda News

News di prodotto

Filters:8

Welcome to the TDK-Lambda news room. Here you'll find all of our product news and corporate announcements. You can also visit our news website for additional TDK-Lambda news.

12W IP66-rated LED power supplies from TDK-Lambda

Postato : 06 Oct 2009

TDK-Lambda has developed a new range of power supplies specifically targeted towards LED applications requiring high reliability. 

Per saperne di più

TDK-Lambda introduces 1kW single-output power supplies in 1U format

Postato : 30 Sep 2009

TDK-Lambda introduces 1kW single-output power supplies in 1U format

Per saperne di più

TDK-Lambda extends NV-Power’s reach

Postato : 08 Sep 2009

TDK-Lambda has expanded its innovative NV-Power family of configurable AC-DC power supplies with the addition of four new output modules

Per saperne di più

TDK-Lambda augments EFE medical range with 28V, 40V and 48V models

Postato : 01 Sep 2009

TDK-Lambda augments EFE medical range with 28V, 40V and 48V models

Per saperne di più

TDK-LAMBDA PUTS THREE-PHASE POWER ON THE RAIL

Postato : 30 Jun 2009

To complement its already highly successful DPP range of DIN-Rail power supplies, TDK-Lambda has introduced three-phase input models.

Per saperne di più

TDK-LAMBDA QUARTER BRICKS MEET POWER-HUNGRY, ATCA REQUIREMENTS

Postato : 28 Apr 2009

TDK-Lambda has expanded its DC-DC converter line-up with the introduction of the new iQG Series, providing exceptionally high true useable power in an industry standard quarter-brick footprint.

Per saperne di più

DESIGN WITH THE LATEST POWER INNOVATIONS USING

Postato : 30 Mar 2009

TDK-Lambda, the innovator in power supply development, has launched its new power products catalogue for 2009

Per saperne di più

TDK-LAMBDA EXPANDS iHG FAMILY OF DOSA HALF BRICKS

Postato : 23 Mar 2009

Following on from the successful launch of the iHG Series of half brick DC-DC converters, TDK-Lambda has added new devices offering a wide input range (36-75V) with nominal outputs from 2.5V/80A (200W), 3.3V/30A (99W), 3.3V/70A (231W), 5V/10A (50W) and 5V/60A (300W).

Per saperne di più

Latest 25W and 35W single output supplies from TDK-Lambda

Postato : 09 Feb 2009

Following on from the successful launch of the LS Series of convection cooled, single output power supplies, TDK-Lambda has added the 25W and 35W models

Per saperne di più

CHALLENGES OF SPACE-SAVING POWER SUPPLIES FOR HARSH ENVIRONMENTS

Postato : 19 Jan 2009

Operating reliably in extreme ambient temperatures is no small task for AC to DC power supplies with PFC, says David Buck of TDK-Lambda Europe, especially when they are employed in indoor and outdoor-mounted electronic equipment where compact size is mandatory

Per saperne di più

ADVANCES IN POWER SUPPLIES FOR AUTOMATED ELECTROCHEMICAL MINI-PLANTS

Postato : 19 Jan 2009

On-site and on-demand production of disinfectants, biocides and water purification chemicals including sodium hypochlorite, chlorine dioxide has been substantially improved via the use of advanced switchmode power supplies that provide the power for automated electrochemical generators

Per saperne di più

TDK-LAMBDA’S AC INPUT FULL-BRICKS TAKE EFFICIENCY TO THE NEXT LEVEL

Postato : 12 Jan 2009

Following the success of the PFE range of AC-DC full-brick power supplies, TDK-Lambda has introduced the PFE-S series with enhanced circuitry to improve lightning surge capability (up to 6kV) and line interrupt hold-up time

Per saperne di più

1 X 1 INCH DC-DC CONVERTERS POWER UP TO 15W

Postato : 05 Dec 2008

TDK-Lambda has added two new models to its already succesful PX family of single- and dual-output 15W DC-DC converters

Per saperne di più

TDK-LAMBDA LAUNCHES FIRST 1000W AC-DC POWER BRICKS

Postato : 28 Nov 2008

TDK-Lambda adds more functionality to its PFE range of AC-DC MEGA-brick power supplies with the introduction of the 1000W PFE-F Series

Per saperne di più

TDK-LAMBDA EXTENDS QUARTER BRICK LINE

Postato : 06 Nov 2008

TDK-Lambda has further extended its impressive line up of high power quarter brick modules with the introduction of the iQL Series

Per saperne di più

DIGITAL CONTROL POWER SUPPLIES FROM TDK-LAMBDA

Postato : 27 Oct 2008

TDK-Lambda has extended its revolutionary digital power supply technology to include a new range of models designed specifically with medical applications in mind

Per saperne di più

TDK-LAMBDA TAKES DIGITAL CONTROL TO THE NEXT LEVEL

Postato : 09 Oct 2008

Taking digital control to the next level, TDK-Lambda’s revolutionary EFE Series of embedded frontend power supplies delivers industry leading power density, high efficiency and enhanced reliability

Per saperne di più

LAMBDA PACKS 2.4kW INTO A 1U RACK

Postato : 29 Jul 2008

Lambda has added a new 1U 2.4kW version to its successful Genesys™ range of rack-mountable, programmable power supplies that cover 1U, 2U and 3U formats

Per saperne di più

LAMBDA'S PFE500F BRINGS MORE FUNCTIONALITY TO THE PFE SERIES

Postato : 17 Jul 2008

Lambda has extended its PFE series of AC-DC full-brick power modules with the introduction of the PFE500F with additional features including active current sharing and remote on/off. Like the existing PFE300, PFE500 and PFE700 models, the new PFE500F versions provide a convenient ac-dc board mounted solution for applications – such as industrial, datacom and telecom – but bring further functionality.

Per saperne di più

POWER SUPPLIES AND CONDUCTED EMISSIONS – 10 QUESTIONS ANSWERED

Postato : 17 Jul 2008

What EMC considerations should an engineer take into account when designing in a power supply? Stuart Nottage and Rob Hutton of Lambda UK give their advice.

Per saperne di più

PAGE TOP

PAGE TOP