Alternatively, you can contact us like this:
Welcome to the TDK-Lambda news room. Here you'll find all of our product news and corporate announcements. You can also visit our news website for additional TDK-Lambda news.
Posted : 14 Dec 2009
Global power supply manufacturer TDK-Lambda has expanded its DC-DC converter line-up with the introduction of the new CN-A Series that have a wide range 60 -160VDC input, which is widely used in railway applications
Read morePosted : 08 Dec 2009
To satisfy customer demand for low power DC-DC converters that can be rapidly mounted onto DIN rails, TDK-Lambda has introduced the DPX Series
Read morePosted : 30 Sep 2009
TDK-Lambda introduces 1kW single-output power supplies in 1U format
Read morePosted : 08 Sep 2009
TDK-Lambda has expanded its innovative NV-Power family of configurable AC-DC power supplies with the addition of four new output modules
Read morePosted : 01 Sep 2009
TDK-Lambda augments EFE medical range with 28V, 40V and 48V models
Read morePosted : 30 Jun 2009
To complement its already highly successful DPP range of DIN-Rail power supplies, TDK-Lambda has introduced three-phase input models.
Read morePosted : 28 Apr 2009
TDK-Lambda has expanded its DC-DC converter line-up with the introduction of the new iQG Series, providing exceptionally high true useable power in an industry standard quarter-brick footprint.
Read morePosted : 30 Mar 2009
TDK-Lambda, the innovator in power supply development, has launched its new power products catalogue for 2009
Read morePosted : 23 Mar 2009
Following on from the successful launch of the iHG Series of half brick DC-DC converters, TDK-Lambda has added new devices offering a wide input range (36-75V) with nominal outputs from 2.5V/80A (200W), 3.3V/30A (99W), 3.3V/70A (231W), 5V/10A (50W) and 5V/60A (300W).
Read morePosted : 09 Feb 2009
Following on from the successful launch of the LS Series of convection cooled, single output power supplies, TDK-Lambda has added the 25W and 35W models
Read morePosted : 19 Jan 2009
Operating reliably in extreme ambient temperatures is no small task for AC to DC power supplies with PFC, says David Buck of TDK-Lambda Europe, especially when they are employed in indoor and outdoor-mounted electronic equipment where compact size is mandatory
Read morePosted : 19 Jan 2009
On-site and on-demand production of disinfectants, biocides and water purification chemicals including sodium hypochlorite, chlorine dioxide has been substantially improved via the use of advanced switchmode power supplies that provide the power for automated electrochemical generators
Read morePosted : 12 Jan 2009
Following the success of the PFE range of AC-DC full-brick power supplies, TDK-Lambda has introduced the PFE-S series with enhanced circuitry to improve lightning surge capability (up to 6kV) and line interrupt hold-up time
Read morePosted : 05 Dec 2008
TDK-Lambda has added two new models to its already succesful PX family of single- and dual-output 15W DC-DC converters
Read morePosted : 28 Nov 2008
TDK-Lambda adds more functionality to its PFE range of AC-DC MEGA-brick power supplies with the introduction of the 1000W PFE-F Series
Read morePosted : 06 Nov 2008
TDK-Lambda has further extended its impressive line up of high power quarter brick modules with the introduction of the iQL Series
Read morePosted : 27 Oct 2008
TDK-Lambda has extended its revolutionary digital power supply technology to include a new range of models designed specifically with medical applications in mind
Read morePosted : 09 Oct 2008
Taking digital control to the next level, TDK-Lambda’s revolutionary EFE Series of embedded frontend power supplies delivers industry leading power density, high efficiency and enhanced reliability
Read morePosted : 29 Jul 2008
Lambda has added a new 1U 2.4kW version to its successful Genesys™ range of rack-mountable, programmable power supplies that cover 1U, 2U and 3U formats
Read morePosted : 17 Jul 2008
Lambda has extended its PFE series of AC-DC full-brick power modules with the introduction of the PFE500F with additional features including active current sharing and remote on/off. Like the existing PFE300, PFE500 and PFE700 models, the new PFE500F versions provide a convenient ac-dc board mounted solution for applications – such as industrial, datacom and telecom – but bring further functionality.
Read more