Gerne können Sie uns auch telefonisch oder per E-Mail erreichen!
Traditional designs that employ distributed power architecture place DC-DC converters on PC boards very close to the point-of-load to maximize system speeds and efficiencies. To power the DC-DC converters, the required AC-DC power supply with PFHC is typically mounted somewhere in the system's enclosure, external to the main pc-board (Figure 1). This technique is quite reasonable for most applications. However, when it comes to equipment that must be mounted outdoors and occupy the smallest possible volume, there are now improved power products available.