U kunt ook op de volgende manier contact met ons opnemen:
Welcome to the TDK-Lambda news room. Here you'll find all of our product news and corporate announcements. You can also visit our news website for additional TDK-Lambda news.
Geplaatst : 01 May 2003
Independent brand awareness studies recently carried out by two of America’s leading electronics magazines, EDN and ECN, both conclude that when it comes to power supplies the number one company of choice is Lambda.
Lees verderGeplaatst : 01 May 2003
World-leading power supply manufacturer Lambda is introducing a new series of AC-DC power supplies that is ideal for cost-sensitive applications that require both high reliability and high performance.
Lees verderGeplaatst : 01 May 2003
Lambda continues to drive up the power density of its PAH family of ‘half-brick’ DC-DC power modules with the introduction of the new PAH300S48 with output voltages of 28 or 12V DC and 300W of power from a single output.
Lees verderGeplaatst : 01 Apr 2003
Leading power solutions manufacturer Lambda has introduced its new CD product catalogue for 2003. ‘Engineering CD 2003’ provides access to in-depth data on a range that includes configurable and standard AC-DC power supplies, both low and high power DC-DC converters, specialist high power programmable supplies and telecom rectifiers.
Lees verderGeplaatst : 01 Mar 2003
Technological advancement in DC-DC converters is continuing apace at Lambda as shown by the new PAQ100H range, the company’s most efficient, highest power quarter-brick DC-DC to-date.
Lees verderGeplaatst : 01 Mar 2003
The Tarka range is a new generation of non-isolated DC-DC converters from leading global power solutions provider Lambda. The first model to be unveiled is the PL10, a 5V input, 10A output single-in-line packaged unit.
Lees verderGeplaatst : 01 Feb 2003
Lambda has unveiled an unpotted version of its X Series of industry standard 2 x 1 sized DC-DC converters. The new 20W UX20 allows designers to take full advantage of forced-air cooling to achieve higher output powers over a wider temperature range.
Lees verderpagina 20 van 20
vorige |