U bent hier  :  home  ››  nieuws  ››  productnieuws

U kunt ook op de volgende manier contact met ons opnemen:

TDK-Lambda Nieuws

Productnieuws

Filters:2

Welcome to the TDK-Lambda news room. Here you'll find all of our product news and corporate announcements. You can also visit our news website for additional TDK-Lambda news.

LAMBDA PUTS MORE POWER ON THE RAIL

Geplaatst : 09 Oct 2006

Extending its DPP range of DIN-Rail power supplies to include new high power models is Lambda.

Lees verder

NOW LAMBDA HAS ALL THE CONVERTERS YOU’LL EVER NEED!

Geplaatst : 04 Oct 2006

Power Supply expert Lambda now provides a truly comprehensive range of products with the addition of the TDK Innoveta family of DC-DC converters following Lambda's acquisition by TDK last year.

Lees verder

LAMBDA’S NEW LOW PROFILE DIN RAIL POWER SUPPLIES FIT THE BOX FOR BUILDING AUTOMATION

Geplaatst : 02 Oct 2006

Just 56mm deep, the new low-profile DSP DIN-rail mounting power supplies from Lambda are specifically designed for easy installation in the shallow cabinets commonly used in building automation and security applications.

Lees verder

LAMBDA LAUNCHES NEW PRODUCT CATALOGUE

Geplaatst : 11 Sep 2006

Lambda, the specialist power supply manufacturer, has launched its new power products catalogue for 2006/2007.

Lees verder

LAMBDA NOW OFFERS TDK DC/DC CONVERTERS

Geplaatst : 04 Sep 2006

The latest CC-E compact DC/DC converters designed and manufactured by TDK are now available from power supply specialists, Lambda under the new collaborative TDK - Lambda product brand.

Lees verder

LAMBDA ADDS MEDICAL AND HEAVY DUTY VERSIONS TO HWS POWER SUPPLY RANGE

Geplaatst : 18 Jul 2006

Lambda, the specialist power supply manufacturer, has now extended it’s industry leading HWS family of compact single-output power supplies to include models that are approved for use in medical equipment.

Lees verder

LAMBDA BOOSTS EMC PERFORMANCE FOR LESS

Geplaatst : 11 Jul 2006

Two new families of very competitively priced filters from Lambda UK make it easy and inexpensive for engineers to enhance the EMC performance of almost any type of electronic equipment.

Lees verder

LAMBDA HAS TOUGH SUPPLIES FOR INDUSTRY

Geplaatst : 07 Jul 2006

Designed to deliver high reliability even in harsh operating conditions, single-output industrial power supplies in the new LZSa series from Lambda combine rugged mechanical construction with an enhanced thermal design that allows them to operate over the exceptionally wide temperature range of -40ºC to +71ºC.

Lees verder

SUPPLYING THE POWER FOR MEDICINE

Geplaatst : 25 Apr 2006

The specification of power supplies for medical applications is a task which needs to be approached with care. In particular, as Andy Skinner of Lambda UK explains, it is never safe to make assumptions about the suitability of power supplies which were primarily designed for industrial use.

Lees verder

COMPACT SUPPLIES FROM LAMBDA MEET MILITARY SPECS!

Geplaatst : 11 Apr 2006

Lambda, the leading global power supply manufacturer, has announced that, after extensive testing, its compact NV-175 and NV-350 multi-output power supplies have been granted approval in line with the stringent demands of US military standard, Mil-Std-801E.

Lees verder

TDK and Densei-Lambda Launch Unified Product Brand

Geplaatst : 27 Mar 2006

Start collaboration with co - marketing activities to enhance power-supply business.

Lees verder

LAMBDA’S NEW NV-175 POWER SUPPLY KEEPS ITS COOL

Geplaatst : 20 Mar 2006

The new integral-fan version of Lambda UK’s ( www.lambda-europe.com) popular NV-175 compact multi-output power supply can deliver its full rated output power continuously, at ambient temperatures as high as 50ºC, even when there is no external source of cooling air flow.

Lees verder

Lambda offers lowest cost of ownership

Geplaatst : 28 Feb 2006

Lambda UK has launched a new version of its FPS1000 front end power supply with a nominal output voltage of 32V adjustable from 28.8 to 38.4.

Lees verder

How do you plan to verify RoHS components?

Geplaatst : 20 Feb 2006

This must be a question most component engineers and purchasers are asking themselves as the RoHS directive implementation date of July 2006 approaches.

Lees verder

Lambda announces 2U 3.3kw addition to Genesys™ family of high density programmable power supplies

Geplaatst : 24 Jan 2006

Lambda has added a new 3.3kW version of its successful Genesys™ range of rack-mountable, programmable power supplies.

Lees verder

Lambda strengthens single output industrial power supply offering with new 300W and 600W versions

Geplaatst : 01 Jan 2006

Lambda extends its range of popular single output industrial power supplies.

Lees verder

LAMBDA INTRODUCES NEW ADDITIONS TO ZP FAMILY

Geplaatst : 28 Nov 2005

Lambda, the global power supply specialist, has extended its ZP range of AC-DC power supplies to include 20W and 100W versions in addition to the existing 40W and 60W units.

Lees verder

LAMBDA extends Front End Power portfolio with NV-350FEP

Geplaatst : 16 Nov 2005

Lambda has added a 350W Front End Power version to its NV-Power range of class-leading, high density and environmentally friendly power supplies.

Lees verder

Lambda DC-DCs deliver distributed power to point-of-load

Geplaatst : 11 Nov 2005

Lambda, the power supply specialists, has extended its range of non-isolated DC-DC converters by adding 5, 16 and 20A models.

Lees verder

Lambda launches new surface mount version of successful PSS & PSD

Geplaatst : 18 Oct 2005

Leading power supply manufacturer Lambda announces a SMT version of its successful PSS and PSD series of ultra compact single and dual DC-DC converters for mounting on printed circuit boards (PCBs).

Lees verder

Komende evenementen

PAGE TOP

PAGE TOP