U kunt ook op de volgende manier contact met ons opnemen:
Welcome to the TDK-Lambda news room. Here you'll find all of our product news and corporate announcements. You can also visit our news website for additional TDK-Lambda news.
Geplaatst : 13 Jan 2009
At this year’s Southern Manufacturing & Electronics show, visitors to the TDK-Lambda stand (C37) will discover all the latest advances and innovations in power technology
Lees verderGeplaatst : 12 Jan 2009
Following the success of the PFE range of AC-DC full-brick power supplies, TDK-Lambda has introduced the PFE-S series with enhanced circuitry to improve lightning surge capability (up to 6kV) and line interrupt hold-up time
Lees verderGeplaatst : 05 Dec 2008
TDK-Lambda has added two new models to its already succesful PX family of single- and dual-output 15W DC-DC converters
Lees verderGeplaatst : 28 Nov 2008
TDK-Lambda adds more functionality to its PFE range of AC-DC MEGA-brick power supplies with the introduction of the 1000W PFE-F Series
Lees verderGeplaatst : 06 Nov 2008
TDK-Lambda has further extended its impressive line up of high power quarter brick modules with the introduction of the iQL Series
Lees verderGeplaatst : 27 Oct 2008
TDK-Lambda has extended its revolutionary digital power supply technology to include a new range of models designed specifically with medical applications in mind
Lees verderGeplaatst : 09 Oct 2008
Taking digital control to the next level, TDK-Lambda’s revolutionary EFE Series of embedded frontend power supplies delivers industry leading power density, high efficiency and enhanced reliability
Lees verderGeplaatst : 29 Jul 2008
Lambda has added a new 1U 2.4kW version to its successful Genesys™ range of rack-mountable, programmable power supplies that cover 1U, 2U and 3U formats
Lees verderGeplaatst : 17 Jul 2008
Lambda UK is showcasing an extensive display of new products, ranging from tiny board-mounting DC-DC converters to multi-kilowatt power supplies, at Southern Electronics 2008.
Lees verderGeplaatst : 17 Jul 2008
Lambda has extended its PFE series of AC-DC full-brick power modules with the introduction of the PFE500F with additional features including active current sharing and remote on/off. Like the existing PFE300, PFE500 and PFE700 models, the new PFE500F versions provide a convenient ac-dc board mounted solution for applications – such as industrial, datacom and telecom – but bring further functionality.
Lees verderGeplaatst : 17 Jul 2008
What EMC considerations should an engineer take into account when designing in a power supply? Stuart Nottage and Rob Hutton of Lambda UK give their advice.
Lees verderGeplaatst : 17 Jul 2008
Lambda UK Stand E60 National Electronics Week Earls Court, London 17th – 19th June, 2008
Lees verderGeplaatst : 09 Jul 2008
Lambda’s new LS Series of convection cooled single output power supplies is available in 50, 75, 100 and 150W models.
Lees verderGeplaatst : 04 Jul 2008
Lambda has launched a lower power range of multi-output models to its popular NV-Power family of configurable power supplies
Lees verderGeplaatst : 30 Jun 2008
Lambda has extended its successful HWS family of single output power supplies with the introduction of the 300W and 600W versions with a 300% peak power capability for 5 seconds
Lees verderGeplaatst : 25 Mar 2008
Lambda has introduced a new range of digitally controlled modules to its innovative NV-Power family of configurable AC-DC power supplies
Lees verderGeplaatst : 25 Feb 2008
Lambda has expanded its half-brick DC-DC converter line-up with the introduction of the new iHG series
Lees verderGeplaatst : 01 Feb 2008
Lambda has added to its range of point of load converters with the launch of the iAD series of non-isolated, single inline package, through-hole mounting devices.
Lees verderGeplaatst : 07 Jan 2008
Lambda Europe has announced that its HWS series of high-quality industrial power supplies now comes with a lifetime warranty as standard, a “first” in the industry.
Lees verderGeplaatst : 18 Dec 2007
Lambda has expanded its already hugely successful SWS series of single output AC-DC power supplies with the introduction of medically-approved 1000W units.
Lees verder