Name:

Email address:
     

Country:

Message:
   

Please leave this empty


Alternatively, you can contact us like this:

Technical Centre

EMC/EMI Filters

How does an input EMI filter work?

Most electronics contains an EMI filter, either as a separate device, or embedded in circuit boards.  Its function is to reduce high frequency electronic noise that may cause interference with other devices.  Regulatory standards exist in most countries that limit the amount of noise that can emitted.
EMI, or Electro-Magnetic Interference, is defined as unwanted electrical signals and can be in the form of conducted or radiated emissions.  Conducted EMI is where the noise travels along the electrical conductors and radiated EMI is where the noise travels through the air as magnetic fields or radio waves.
EMI is generated from the switching of electrical current and comes from a variety of sources including electronic power supplies.  Power supplies convert an input voltage into regulated and isolated (in most cases) DC voltages to run a host of electronic components.  That conversion is performed at high frequencies ranging from several kHz to more than a MHz.  LED lighting, computers, motor drivers, DC relays and battery chargers all rely on power supplies to operate.

An EMI filter for a power supply normally consists of passive components, including capacitors and inductors, connected together to form LC circuits.  The inductor(s) allow DC or low frequency currents to pass through, while blocking the harmful unwanted high frequency currents.  The capacitors provide a low impedance path to divert the high frequency noise away from the input of the filter, either back into the power supply, or into the ground connection.

In addition to assisting to meet EMI regulations, the filter also has to meet safety standards.  The inductor temperature rise is measured and for mains operation, the minimum electrical spacing between line, neutral and ground are controlled.  This reduces the risk of fire and electrical shock.  The capacitors are also individually safety certified, depending on their position in the circuit.  Special “X” capacitors have to be used across the input terminals and “Y” capacitors from the AC circuit to ground.



Figure 1 shows a simple single stage power supply filter

Additional Information:

Additional Technical Centre Resources

PAGE TOP