TDK-Lambda zeichnet dataTec aus
13 Jul 2015
TDK-Lambda hat seinen Vertriebspartner dataTec mit dem »Outstanding Sales ... Umsatzwachstumsraten beim Verkauf von TDK-Lambdas Stromversorgungen über einen Zeitraum von vier Jahren.
Read more
700W AC/DC powermodul › Power, strømforsyning, EMC/ESD
19 Feb 2015
700W AC/DC powermodulTDK-Lambda PFE-SA serien af AC/DC full-brick powermoduler udvides med 700W ... introduces a 700W model to the TDK-Lambda PFE-SA series of AC/DC full-brick power modules. A significant...
Read more
100W single output AC/DC forsyning til krævende applikationer › Power...
22 Jan 2015
...english).TDK Corporation announces that TDK-Lambda has introduced the ZMS100, the first unit in the ZM series of ... Southam, Director of Marketing for TDK-Lambda EMEA.Meticulous design has maximised electrolytic capacitor...
Read more
TDK-Lambda lancerer nye single-output AC/DC strømforsyninger...
24 Nov 2014
TDK-Lambda lancerer nye single-output AC/DC strømforsyningerTDK-Lambda udvider med RWS-B... Available in five power levels between 50W and 600W, the TDK-Lambda RWS-B models operate from a universal...
Read more
800W high-voltage programmable DC power supply
18 Nov 2014
...ProphetTDK’s 800W model in the TDK-Lambda Z+ series of high voltage programmable DC power supplies is ... designed to meet UL/EN60950-1.TDK-Lambda; www.uk.tdk-lambda.com/zplusPower Supplies/Batteries,Test...
Read more
Programmable Power Supplies
10 Oct 2014
...models have been added to its TDK-Lambda Z+ Series of programmable DC power supplies. Complementing the ... may be connected in series.TDK-Lambda EMEAKingsley Avenue EX34 8ES Ilfracombe United Kingdom...
Read more
AC/DC 'full brick' powermoduler med høj effektivitet › Power, strømforsyning...
18 Aug 2014
...powermoduler med høj effektivitet TDK-Lambda introducerer PFE-SA serien af AC/DC 'full-brick' power moduler... TDK Corporation introduces the TDK-Lambda PFE-SA series of AC-DC full-brick power modules, which represents...
Read more
Programmable power supplies deliver up to 650 VDC
16 Jul 2014
...EE Times Europe -July 16, 2014 The Z+ high-voltage series from TDK Lambda extends the company's line-up. It comes with a choice of with output voltages of up to 160 VDC, 320 VDC or 650 VDC. These higher...
Read more
Programmable power supplies deliver up to 650Vdc
15 Jul 2014
...2014 // Christoph Hammerschmidt The Z+ high voltage series from TDK Lambda extends the company's line-up. It comes with a choice of with output voltages of up to 160, 320 or 650Vdc. These higher voltages...
Read more
Power Supply firm invests in North Devon
01 May 2014
com Power Supply firm invests in North Devon TDK-Lambda UK is continuing to invest heavily in its North... The decision to invest further is fuelled by TDK-Lambda’s future plans for product development and...
Read more
Ac-dc Power Supplies
10 Apr 2014
...whereas the higher power models incorporate an internal cooling fan. TDK-Lambda EMEA Kingsley Avenue EX34 8ES Ilfracombe United Kingdom : +44-1271-856600 : +44-1271-864894 Programmable Power Supplies Include...
Read more
HVDC bus DC-DC modules are conduction-cooled
25 Mar 2014
TDK-Lambda PH-A280 series DC-DC power modules are suitable for high input ... fanless construction and compact. TDK-Lambda; www.uk.tdk-lambda.com/ph-a
Read more
Lighter AC-DC power supplies deliver performance improvements
14 Nov 2013
...Corporation has introduced the TDK-Lambda HWS-A series of AC-DC power supplies, which comprises five models ... conducted and radiated EMI. The TDK-Lambda HSW-A series is approved to UL/CSA/EN 60950-1 and UL508 (with...
Read more
TDK-Lambda - New 300W model augments ZWS-BAF series of AC-DC power ...
22 Feb 2013
TDK-Lambda ZWS-BAF series of single-output power supplies has been expanded with the addition of a new 300W model. The ZWS300BAF operates from a universal input of 85 to 265VAC or 120-370VDC and features a 10-year E-cap lifetime for superior ...
Read more
TDK-Lambda opens Advanced Technology Centre in Bristol — LED ...
19 Jan 2013
TDK Corporation announces the opening of TDK-Lambda's new EMEA Advanced Technology Centre (ATC) in Bristol. Located at the Bristol and Bath Science ...
Read more